Hello,Sorry for the long delay, I can understand your frustation.Concerning the FTP programming, you can find the answer in the GUI user manual:https://www.st.com/en/embedded-software/stsw-wpstudio.html#documentationYou have 2 ways to modify the para...
Hello,The output voltage from STWLC38 is not supposed to oscillate, it should be stable as it is a LDO output.Could you attach a zoom of the period of time where VIN2=5V and then it falls ? It is difficult to see on the plot the behavior of VIN2 and ...
Hello,No, you do not need to send any init command to get the chipset ready.Nevertheless, you need to enable the "Data latch" to get the values latched in the data register (see register dsp_cr3):either by enabling the automatic SW latch (bit 23): th...