cancel
Showing results for 
Search instead for 
Did you mean: 

Connection between custom board with lsm6dso32x and unico gui tool

sygo
Associate II

I am currently using the LSM6DSO32X sensor on a custom board.

 

I want to connect a custom board to the Unico GUI tool and utilize its features. Is it possible?

 

If possible, how can I achieve that?

thank you

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Federica Bossi
ST Employee

Hi @sygo ,

UNICO-GUI is a user interface interacting with STEVAL-MKI109V3, the motherboard compatible with all ST MEMS adapter boards.

You find all the documentations to work with Unico properly here.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.