User Activity

Hi I have an urgent issue.I cant seem to be able to change some settings on the MCUsPCROP1_STRT 0x7FFFPCROP1_END 0x7FFFPCROP_RDP is checkedPCROP2_STRT 0x7FFFPCROP2_END 0x7FFFI cant change them. If i try i get12:32:21 : Error: Expected value for Optio...
Hi Using FreeRTOS V11.0.1 and Stm32Cubeide 1.14.1 I was trying to read out the percentage information into the debugger.  Unfortunately I don't get the expected behaviorAs all of my tasks are either below 1% or at 1%, it does not seem correct.I have ...
Hi Could you please change the library implementations so that  void __stack_chk_fail(void)andunsigned long __stack_chk_guardare defined as weak?I have tested it with GCC 11.3.rel1 and 12.3.rel1 and on both i get "multiple definitions of __stack_chk_...
HiEarlier today I was demonstrating a IAP functionallity with dualbanking on a stm32G474RET. I was saying that it cannot fail as I check the written image with a CRC after it has been written to the new bank.As I power of the system mid transfer and ...
HiAssume that i set up an H-bridge and and control it via the HRTIM block and use the build in deadtime features. I then also enable a couple of faults. The bridges safe state will be to set both lower transistors to be OFF and the two upper once to ...
Kudos given to