2024-05-07 8:46 PM
Hi
I have an urgent issue.
I cant seem to be able to change some settings on the MCUs
PCROP1_STRT 0x7FFF
PCROP1_END 0x7FFF
PCROP_RDP is checked
PCROP2_STRT 0x7FFF
PCROP2_END 0x7FFF
I cant change them. If i try i get
12:32:21 : Error: Expected value for Option Byte "PCROP1_END": 0x0, found: 0x7FFF
12:32:21 : Error: Expected value for Option Byte "PCROP_RDP": 0x0, found: 0x1
12:32:21 : Error: Option Byte Programming failed Or modified by application after OB_LAUNCH
How can i recover this?
Please contact me as soon as possible!
Best regards
Martin
2024-05-07 10:36 PM
UPDATE
I managed to fix this by temporarily change it into a single bank, instead of the dual bank i normally had. After changeing and applying this, i could change the now single values for PCROP and apply them. After that change it back to a dual bank.
Best regards
Martin