cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U585 : ADC4 configuration

MFred.2
Associate III

With this configuration :

  • nbr of conversion : 2
  • scan conversion mode : Enable
  • Continious Conversion Mode : cannot set to Enable !!!
  • Discontinious Conversion Mode : ucannot set to Disable !!!

Unless I am mistaken, I see no indication in the STM32U5 reference manual that does not allow this configuration (Scan conversion and Continuous Conversion).

I guess a cubeMX bug?

STM32CubeIDE 1.9.0, STM32CubeMX : 6.5.0-RC4,

STM32U5 package version 1.1.0.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Sara BEN HADJ YAHYA
ST Employee

Hello @MFred.2​ ,

Thanks for raising this issue to our attention,

Issue confirmed from my side and I reported it to the dev team to fix it asap.

Internal ticket number: 128661(This is an internal tracking number and is not accessible or usable by customers).

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Sara BEN HADJ YAHYA
ST Employee

Hello @MFred.2​ ,

Thanks for raising this issue to our attention,

Issue confirmed from my side and I reported it to the dev team to fix it asap.

Internal ticket number: 128661(This is an internal tracking number and is not accessible or usable by customers).

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Sara BEN HADJ YAHYA
ST Employee

 Hello @MFred.2​ ,

This issue is fixed in STM32CubeMX latest release.

V6.6.0 is now available under this Link.

Thanks for your contribution.

Sara.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.