Hi @VT_Jim indeed the SD has its own internal DMA as soon as you are using the HAL_SD_XXX_DMA() API then it is O.K.https://github.com/STMicroelectronics/x-cube-azrtos-h7/blob/f48d941bcbe270bcb0b01c0fcedd3924db778d42/Projects/STM32H735G-DK/Application...
Hi @xixi,since the flag TX_EXECUTION_PROFILE_ENABLE is being used in ".S" you'll need to add that define in the assembly preporcessor rather than the C/C++ one. regardsHaithem.
Hi @Kai_Satone it seems that you are setting the configKERNEL_PROVIDED_STATIC_MEMORY to 1 in your FreeRTOSConfig.h fileif it is the case then please unset it. It is clearly stated in FreeRTOS comments below.https://github.com/FreeRTOS/FreeRTOS-Kernel...
Hi @Pajaka,After checking further, you'll be able to solve your issue. when calling fx_media_abort(), the macro FX_STM32_SD_POST_ABORT(_media_ptr) https://github.com/STMicroelectronics/STM32CubeU5/blob/f0f063146b444e37ef6b1b3d2f219df728a12407/Project...