User Activity

Hi AllGreetingsIm using the SBSFU folder from b-U585-IOT2A and was successfully running the codes. When updated the cube ide to latest version v1.18 from version v1.17, the following compilation is occuring in the Secure ApplicationError message:"C:/...
Hi @Jocelyn RICARD GreetingsWe have a query from our support team"known vulnerability in the STM32U5 series related to the JTAG lock when using RDP (Readout Protection) Level 2." Is it advisable to proceed with this implementation, or should we consi...
Hi @Jocelyn RICARD Greetingswe are trying to run TFM example (with secure and non secure project) taken from GPIO_Toggle_TZEN Example and adding SPI communication in the non secure project on our custom board mounted with STM32U585aii6q controller SP...
Hi @Jocelyn RICARD Greetingswe are working on the STM32u585 TFM Application and are facing issues when running the code. the issue is after dumping the code using the TFM_Update.sh script first time every operation is normal, but while running for th...
Hello communityGreetingsi have a requirement to write and read data from the SRAM2 and Backup RAM from the TFM Application example. please suggest how can i write and read an array of bytes(10 byte) from the SRAM2 and Backup RAM in the above mentione...
Kudos from