2024-05-24 02:56 PM
Version: 2.0.1
Steps to reproduce: Create empty project for NUCLEO-F767ZI, vector table in startup code will be incorrect.
/******************************************************************************
*
* The STM32F767ZITx vector table. Note that the proper constructs
* must be placed on this to ensure that it ends up at physical address
* 0x0000.0000.
*
******************************************************************************/
.section .isr_vector,"a",%progbits
.type g_pfnVectors, %object
g_pfnVectors:
.word _estack
.word Reset_Handler
.word NMI_Handler
.word HardFault_Handler
.word 0
.word 0
.word 0
.word 0
.word 0
.word 0
.word 0
.word SVC_Handler
.word 0
.word 0
.word PendSV_Handler
.word SysTick_Handler
.word HASH_RNG_IRQHandler /* Hash and Rng global interrupt */
.word CRYP_IRQHandler /* CRYP crypto global interrupt */
.word DCMI_IRQHandler /* DCMI global interrupt */
.word FMC_IRQHandler /* FMC global interrupt */
.word DMA2_Stream0_IRQHandler /* DMA2 Stream0 global interrupt */
.word DMA2_Stream1_IRQHandler /* DMA2 Stream1 global interrupt */
.word DMA2_Stream2_IRQHandler /* DMA2 Stream2 global interrupt */
.word DMA2_Stream3_IRQHandler /* DMA2 Stream3 global interrupt */
.word DMA2_Stream4_IRQHandler /* DMA2 Stream4 global interrupt */
.word DMA2_Stream5_IRQHandler /* DMA2 Stream5 global interrupt */
.word DMA2_Stream6_IRQHandler /* DMA2 Stream6 global interrupt */
.word DMA2_Stream7_IRQHandler /* DMA2 Stream7 global interrupt */
.word DMA1_Stream0_IRQHandler /* DMA1 Stream0 global interrupt */
.word DMA1_Stream1_IRQHandler /* DMA1 Stream1 global interrupt */
.word DMA1_Stream2_IRQHandler /* DMA1 Stream2 global interrupt */
.word DMA1_Stream3_IRQHandler /* DMA1 Stream3 global interrupt */
.word DMA1_Stream4_IRQHandler /* DMA1 Stream4 global interrupt */
.word DMA1_Stream5_IRQHandler /* DMA1 Stream5 global interrupt */
.word DMA1_Stream6_IRQHandler /* DMA1 Stream6 global interrupt */
.word DMA1_Stream7_IRQHandler /* DMA1 Stream7 global interrupt */
.word RCC_IRQHandler /* RCC global interrupt */
.word SPI1_IRQHandler /* SPI1 global interrupt */
.word SPI2_IRQHandler /* SPI2 global interrupt */
.word SPI4_IRQHandler /* SPI 4 global interrupt */
.word SPI5_IRQHandler /* SPI 5 global interrupt */
.word SPI3_IRQHandler /* SPI3 global interrupt */
.word SPI6_IRQHandler /* SPI 6 global interrupt */
.word ADC_IRQHandler /* ADC1 global interrupt */
.word WWDG_IRQHandler /* Window Watchdog interrupt */
.word TIM1_BRK_TIM9_IRQHandler /* TIM1 Break interrupt and TIM9 global interrupt */
.word TIM1_UP_TIM10_IRQHandler /* TIM1 Update interrupt and TIM10 */
.word TIM1_TRG_COM_TIM11_IRQHandler /* TIM1 Trigger and Commutation interrupts and TIM11 global interrupt */
.word TIM1_CC_IRQHandler /* TIM1 Capture Compare interrupt */
.word TIM8_BRK_TIM12_IRQHandler /* TIM8 Break interrupt and TIM12 global interrupt */
.word TIM8_UP_TIM13_IRQHandler /* TIM8 Update interrupt and TIM13 global interrupt */
.word TIM8_TRG_COM_TIM14_IRQHandler /* TIM8 Trigger and Commutation interrupts and TIM14 global interrupt */
.word TIM8_CC_IRQHandler /* TIM8 Capture Compare interrupt */
.word TIM2_IRQHandler /* TIM2 global interrupt */
.word TIM3_IRQHandler /* TIM3 global interrupt */
.word TIM4_IRQHandler /* TIM4 global interrupt */
.word TIM5_IRQHandler /* TIM5 global interrupt */
.word TIM6_DAC_IRQHandler /* TIM6 global interrupt, DAC1 and DAC2 underrun error interrupt */
.word TIM7_IRQHandler /* TIM7 global interrupt */
.word ETH_IRQHandler /* Ethernet global interrupt */
.word ETH_WKUP_IRQHandler /* Ethernet Wakeup through EXTI line */
.word CAN1_TX_IRQHandler /* CAN1 TX interrupts */
.word CAN1_RX0_IRQHandler /* CAN1 RX0 interrupts */
.word CAN1_RX1_IRQHandler /* CAN1 RX1 interrupts */
.word CAN1_SCE_IRQHandler /* CAN1 SCE interrupt */
.word CAN2_TX_IRQHandler /* CAN2 TX interrupts */
.word CAN2_RX0_IRQHandler /* CAN2 RX0 interrupts */
.word CAN2_RX1_IRQHandler /* CAN2 RX1 interrupts */
.word CAN2_SCE_IRQHandler /* CAN2 SCE interrupt */
.word CAN3_TX_IRQHandler /* CAN3 TX interrupt */
.word CAN3_RX0_IRQHandler /* CAN3 RX0 interrupt */
.word CAN3_RX1_IRQHandler /* CAN3 RX1 interrupt */
.word CAN3_SCE_IRQHandler /* CAN3 SCE interrupt */
.word FLASH_IRQHandler /* Flash global interrupt */
.word PVD_IRQHandler /* PVD through EXTI line detection */
.word TAMP_STAMP_IRQHandler /* Tamper and TimeStamp interrupts through the EXTI line */
.word EXTI0_IRQHandler /* EXTI Line0 interrupt */
.word EXTI1_IRQHandler /* EXTI Line1 interrupt */
.word EXTI2_IRQHandler /* EXTI Line2 interrupt */
.word EXTI3_IRQHandler /* EXTI Line3 interrupt */
.word EXTI4_IRQHandler /* EXTI Line4 interrupt */
.word EXTI9_5_IRQHandler /* EXTI Line[9:5] interrupts */
.word EXTI15_10_IRQHandler /* EXTI Line[15:10] interrupts */
.word RTC_ALARM_IRQHandler /* RTC alarms through EXTI line 18 interrupts */
.word OTG_FS_WKUP_IRQHandler /* USB On-The-Go FS Wakeup through EXTI line interrupt */
.word OTG_HS_EP1_OUT_IRQHandler /* USB On The Go HS End Point 1 Out global interrupt */
.word OTG_HS_EP1_IN_IRQHandler /* USB On The Go HS End Point 1 In global interrupt */
.word OTG_HS_WKUP_IRQHandler /* USB On The Go HS Wakeup through EXTI interrupt */
.word OTG_HS_IRQHandler /* USB On The Go HS global interrupt */
.word LCD_TFT_IRQHandler /* LTDC global interrupt */
.word LCD_TFT_1_IRQHandler /* LCD-TFT global Error interrupt */
.word SAI1_IRQHandler /* SAI1 global interrupt */
.word SAI2_IRQHandler /* SAI2 global interrupt */
.word DMA2D_IRQHandler /* DMA2D global interrupt */
.word QuadSPI_IRQHandler /* QuadSPI global interrupt */
.word SPDIFRX_IRQHandler /* SPDIFRX global interrupt */
.word SDMMC1_IRQHandler /* SDMMC1 global interrupt */
.word SDMMC2_IRQHandler /* SDMMC2 global interrupt */
.word LP_Timer1_IRQHandler /* LP Timer1 global interrupt */
.word I2C1_EV_IRQHandler /* I2C1 event interrupt */
.word I2C1_ER_IRQHandler /* I2C1 error interrupt */
.word I2C2_EV_IRQHandler /* I2C2 event interrupt */
.word I2C2_ER_IRQHandler /* I2C2 error interrupt */
.word I2C3_EV_IRQHandler /* I2C3 event interrupt */
.word I2C3_ER_IRQHandler /* I2C3 error interrupt */
.word I2C4_EV_IRQHandler /* I2C4 event interrupt */
.word I2C4_ER_IRQHandler /* I2C4 Error interrupt */
.word RTC_WKUP_IRQHandler /* RTC Tamper or TimeStamp /CSS on LSE through EXTI line 19 interrupts */
.word USART6_IRQHandler /* USART6 global interrupt */
.word USART1_IRQHandler /* USART1 global interrupt */
.word USART3_IRQHandler /* USART3 global interrupt */
.word USART2_IRQHandler /* USART2 global interrupt */
.word UART5_IRQHandler /* UART5 global interrupt */
.word UART4_IRQHandler /* UART4 global interrupt */
.word UART8_IRQHandler /* UART 8 global interrupt */
.word UART7_IRQHandler /* UART7 global interrupt */
.word OTG_FS_IRQHandler /* USB On The Go FS global interrupt */
.word MDIOS_IRQHandler /* MDIO slave global interrupt */
.word DFSDM1_FLT0_IRQHandler /* DFSDM1 Filter 0 global interrupt */
.word DFSDM1_FLT1_IRQHandler /* DFSDM1 Filter 1 global interrupt */
.word DFSDM1_FLT2_IRQHandler /* DFSDM1 Filter 2 global interrupt */
.word DFSDM1_FLT3_IRQHandler /* DFSDM1 Filter 3 global interrupt */
.word JPEG_IRQHandler /* JPEG global interrupt */
.word DSIHOST_IRQHandler /* DSI host global interrupt */
.word FPU_IRQHandler /* FPU global interrupt */