User Activity

Hello friends!Im devloping GUI using TouchGFX on waveshare OpenH7XXI-C board. When im flashing the code. GUI image is getting splitted  from middel.Touchgfx GUI:LCD output  
hello friends!Now a days i started working on TouchGFX for Waveshare's OpenH7XXI-C board and CoreH7XXI MCU. I interfaced 7 inch display, FMC SDRAM as bank 2 and W25Q128 QSPI. after configuring these peripherals i tested them manually by writing and r...
Hello guys! we generally configures UART in the cube mx and generating the codes, and after by calling Transmit and Recieve functions we are checking the outs on serial terminals.. if we dont get desired outputs then we are trying to dubbug and testi...
Hello Community!Now a days i started Working on STM32H747 Discovery board. im trying to configure Ethertnet on Cortex-M7 core.i enabaled ETH in connectivity with RMII on M7 core. Selected FreeRTOS with CMSIS V2 and enabled the DCache. now when im try...
Hello Community!Recently i have started working on USB MSC using RTOS. Im using USB HOST Library version 3.5.2 and latest version of CubeMx.When im generating the code by selecting FreeRTOS CMSIS V2 and pulging my USB drive to CN13 connector then the...