cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H743 SRAM physical specification

RK.1
Associate II

Hi

I am planning to run a RAM test on STM32h743 RAM module. But I noticed that the RAM is divided into 3(SRAM 1,2,3) .Are these three RAMs physically different or the same RAM divided into three modules.

Thanks in Advance

2 REPLIES 2

Distinct arrays, on the same silicon, multiple buses to reduce contention. Actually more RAM than those 3, also SRAM4, AXI RAM, ITCM RAM, DTCM RAM

0693W000004IihpQAC.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
DFuchs
Associate III

I treat them as different RAMs because they have their own row and column decoder.