User Activity

Our design involves storing the images in external flash. Images are fetched in run time from external flash and displayed on LCD. Is there a built-in integrity check to verify the validity of the bitmap before displaying on the LCD?A question came u...
I am wondering if it is possible to implement a screenshot feature with TouchGFX. I want to capture the screen, in jpg or bmp format, and dump the image to serial for later viewing on computer.
I am trying to implement dynamic QRCode generation. I am using the library https://github.com/ricmoo/QRCode and the QRCode widget from https://support.touchgfx.com/4.16/docs/development/ui-development/touchgfx-engine-features/custom-widgets#example-s...
I am using 4.16.1 TouchGFX designer tool. Is it possible to generate QR code for a given string and PIN code in run time and display? Please advice.
I have a setting which can be manually or automatically adjusted/changed. A toggle button selection choses manual or automatic adjustment. Manual adjustment is done using a slider widget. When the toggle button is selected to automatic position, slid...
Kudos from