Hi Ulysses,Thank you to pinpoint that smart cards / java cards are ISO/IEC 14443 interfaces, because ST25 tags with Energy Harvesting feature are only on ISO 15693 standard.Kind Regards.
Hi praveenbm5,I cannot answer for the ST33 Secure MCU and you should contact the local sales for that product to get more information as this is not a public product.Regarding the ePaper, the power required when updating the screen can be provided by...
Hi eagles64,Can I put multiple function records in one NDEF file?For example, I just want to connect uri link with one NDEF file and also wifi connection at the same time.Is it possible? Yes it's possible, 1 NDEF file can include multiple records. If...
Hi Kris-kappa,Following link is an Application note providing information about energy harvesting with ST25DV series (to help you a bit more):https://www.st.com/content/ccc/resource/technical/document/application_note/group0/c2/1f/83/75/2c/f1/41/78/D...
Hi VColi.1,If you want to bypass the Tag detection at demo boot you will have to comment some code and rebuild the firmware.Commenting these lines in the main.c should do the trick : if( ST25DV_pwm == 0 )
{
ST25_RETRY(BSP_NFCTAG_Init(BSP_NFCTA...