2024-12-18 08:31 AM - last edited on 2024-12-18 08:48 AM by Andrew Neil
I have a NUCLEO -G071RB board with an X-NUCLEO-GFX01M2 display shield, and am trying to run the X-CUBE-DISPLAY demonstration software GFX01M2_HelloWorld. I have imported the project to CubeIDE and built it OK, but when I try to run it I get an error "failed to erase memory" (details attached). This happens with CubeIDE 1.15.1 and also with 1.17.0.
Running the example GPIO_IOToggle on the G071RB board loads and runs OK, the problem is only with the GFX01M2 demonstrator.
Am I missing something or am I looking at a board faulty out of the box?
Solved! Go to Solution.
2024-12-18 11:12 AM
Yes I was missing something.
The GFX01M2 was plugged in back to front, which would appear to be fatal to it.
How embarrassing.
2024-12-18 11:12 AM
Yes I was missing something.
The GFX01M2 was plugged in back to front, which would appear to be fatal to it.
How embarrassing.