I want to use the bootloader feature (via UART) of the STM32L071RB. I have read the AN2606 and AN3155.If I'm right, the STM32L071RB has a V11.x bootloader and can be updated via UARTx, SPIx,and I2Cx.Is is possible to configure, which pins are used by...