User Activity

There are several kinds of IPM, but it seems all 3 phase output.Is there any IPM can do single phase motor control and how much is maximum output?  
We have a more than 10 years old STM32F100 project which was built by AC6, I try to use TruStudio and STM32CubeIDE 1.6.1 to import , and build it, but all fails on Error "Program "make" not found in path". How to fix it?
I start the safety functional software by the example from "STM32CubeExpansion_STL_G0_V1.1.0". From the readme.txt, it mention "Install ST CRC tool", but it is "STM32CubeProgrammer", is this tool has built in CRC function? by post-build steps command...
I'm using TrueStudio for my previous product coding/debugging.  I downloaded some example projects from ST website,  there are options for IAR/Keil/STM32CubeIDE, is TrueStudio fully replaced by STM32CubeIDE?I'm get used to TrueStudio, is STM32CubeIDE...
Try to use STM32G0 LQFP32 MCU do accuracy frequency measurement, but there is no HSE crystal interface, so internal HSI RC will be for system clock, the accuracy of the system clock will affect the frequency, how accuracy is internal HSI RC clock
Kudos from