Posted on November 27, 2017 at 03:45 I need to update the SPC5 4.0 project to SPC5 5.6 project. But there is no SPC560Pxx IRQ component RLA in SPC5 5.6.
Posted on November 27, 2017 at 01:24I use the SPC5 Studio 5.6 to open an old project and get the following error.08:20:06 **** Build of configuration Default for project BZW111A_CAT_MHE_Gamma ****make all Compiler Optionsppc-freevle-eabi-gcc -c -mcp...
Posted on November 06, 2017 at 01:37After MCU reset, I got the following and the IOT bit is set. But according to the RM0046(Reference manual, September 2013, Rev 5) the IOT bit should be reset after MCU reset.#lintcsr
Posted on November 29, 2017 at 10:11 For the last reply Nov 29, 2017 9:49 AM, I put the wrong log and then I update the log. I use SPC5 5.6 to create a new project not use the SPC5 5.6 open a SPC5 4.0 old project. Now I do it again and I put the ne...
Posted on November 29, 2017 at 09:43 I changed the IRQ number and the error is still there. I put the log in the attachment.
________________
Attachments : .log.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db00...
Posted on November 29, 2017 at 02:20If I add the following two IRQ, there will be an error everytime. If I don't add the following two IRQ, there will be no error.