User Activity

I use stm32h563 project with netxduo and need to set 1ms timer for rtos time base.After changing  TX_TIMER_TICKS_PER_SECOND to 1000 and NX_IP_PERIODIC_RATE to 1000 and generating new files from ioc i see following:problem # 1TX_TIMER_TICKS_PER_SECOND...
Hi,when I write 8byte block sequentially 256 times in 2kB page and then erase and start over what is the total number of writes I can do?Datasheet describes 10000 write/erase cycles, but I do not erase after every write.If the damage is cause by eras...
Hi, is there support of azure rtos for stm32h5 devices?I am looking for a MCU with ethernet and azure rtos support. I have fond some examples for sym32h7 devices but those are too big. Smallest is 100pins and they are more expensive. The smallest and...
Hi, I have a board with STM32G071KBU6N with new and empty flas.I have difficulty programming it because it seems to set some pins as output after power up. for example PA6 and PB7. This is causing a over current in the circuit.I suspect some kind of ...
Hi. I have recently updated to latest version 1.12.0 and there seems to be some problem with code generator.There is no handler for RTOS systick or for HAL timer. in stm32g0xx_it.cThis was broken for F072 family in the past, but now it is also broken...