Hi @Marudhupandian,
>> Q1: So please clarify this MCU has secure boot options.
Yes this MCU has secure boot options. The main boot options used in the STM32F4 for secure boot and secure firmware update are the following:
MPU privilege access, flash ...
Hi @AnoopYadav
The XSPI2_HSLV can be done by user code as described in RM0477 section 5.4.3 Option byte words modification / Changing option byte words. VDDIO_HSLV option bit is also required with XSPI2_HSLV.
The flash driver provide the following H...
Hello @efthym
Thank you for your important analysis. I shared your feedback with internal STM32 VS Code team.
(Submitted Ticket is 189230, this tracking number is for internal tracking)
Best regards
Hello @alister,
Thank you for your valuable analysis and reporting,
For the typo in "DS14359 Rev 2" I submitted Ticket 189228 (Note that ticket number is for internal tracking only, not accessible externally).
Thanks @Ghofrane GSOURI, I let you ha...
Hi @Istillaga
In non-secure application project you changed the system clock from 160 Mhz to 64 Mhz, then the application doesn't work.
Can you clarify what is the issue ? for example nothing is displayed by tera-term or you get a hardfault .....
...