User Activity

While the Coarse calibration in RTCv2 is obsolete, in 'L1 and 'F2 it's the only method (and I know 'L1 is NRND, but it's still around and will be for years to come, if ST sticks to its commitment), and as long as it's mentioned in 'F4 it should be pr...
Through the Characteristics chapter of L78XX DS, the page break is placed incorrectly so, that the conditions - and sometimes also the first row of the table itself - is at the preceding page. Yes, it's formally OK, but is this how ST intends to pres...
(Spotted by sx107.)I know the subject is not very descriptive, but a figure is worth 1000 words:It's also in other 'H7 RMs; I leave it to ST to check them all :)(Btw. this is a carryover from the 'F7 RM, where both OTG's SOF indeed feed into TIM2 ITR...
The infographics displaying all Nucleo boards at once is missing from https://www.st.com/en/evaluation-tools/stm32-nucleo-boards.html . JW
This is new. I've used it in the past and downloaded data with no problem.Yes, I do have network connection - this post from the very same PC at the moment.JW