cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am new to using stm8 and i have faced a problem while building the project.

XLow
Associate

This is the error message that i have received.

#error clnk Release\ild004v2.lkf:62 Release\smart_reset.o: symbol __stext multiply defined (C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Lib\crtsi0.sm8)

#error clnk Release\ild004v2.lkf:62 Release\smart_reset.o: symbol _exit multiply defined (C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Lib\crtsi0.sm8)

 The command: "clnk -l"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Lib" -o Release\ild004v2.sm8 Release\ild004v2.lkf " has failed, the returned value is: 1

exit code=1.

There is no problem when i build under debug. However this shows up when i build it under release.

The code that I am trying to build is STEVAL-ILD004V2.

The photo attached is the error message I got when I pressed start debugging.

2 REPLIES 2
AvaTar
Lead

What problem, exactly ?

sorry i thought i have added the details. I have just added them.