cancel
Showing results for 
Search instead for 
Did you mean: 

FlexLM No such feature exists

Ivan Yu
Associate
Posted on January 29, 2018 at 17:02

When I try to compile my project or the standard project, I get the message -clDebug \ -coDebug \ main.c #error cpstm8 C: \ Program Files (x86) \ COSMIC \ CXSTM8_32K \ Hstm8 \ mods0.h: 1 FlexLM No such feature exists.I copied the license file to the correct folder, Cosmic CxSTM8 32K and STToolset were installed on the PC. The error is present on two different systems XP and Win7. Reinstalling software does not solve the problem. How can I fix this problem?

1 REPLY 1
luca239955_stm1_st
Senior II
Posted on January 29, 2018 at 18:53

Hello,

the 32k version you are trying to use is old and not supported anymore: get the new version without any limit

http://cosmicsoftware.com/download_stm8_free.php

and the problem will go away.

Regards,

Luca