2019-05-22 07:51 AM
2019-05-22 07:54 AM
Target->Settings, a Settings window opens:
JW
2019-05-22 07:57 AM
I haven't that option on the list, i only have Normal and Hot Plug options
2019-05-22 07:58 AM
And i also can't modify the frequency in the port configuration section
2019-05-22 07:58 AM
Not much to work with here. Doesn't find the ST-LINK? Doesn't find the Target the ST-LINK is attaching too?
What version of the Utility? What board or ST-LINK pod involved.
2019-05-22 08:00 AM
It find ST-LINK, version V1, i am using an stm8s discovery demoboard
2019-05-22 12:41 PM
Ah, V1 has its limitations...
But you should be able to do "connect under reset" also "manually" - hold the NRST line low, while attempting to connect. If it does not work, you have a serious problem.
Is the original target (the STM8) disconnected? Do you use a short cable to connect to the STM32 target?
JW