2019-01-07 2:00 AM
#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\modsl0.h:1 FlexLM No such feature exists.
i am using FSE_Compiler.
How can I fix this problem?
2019-01-07 2:06 AM
Maybe FlexLM relates to toolchain license, to renew, or the memory model used to compile is not useable.
2019-01-07 2:08 AM
What can i do fix it?
Do you have any offer?
2019-01-07 2:11 AM
Software of modslo.h is:
/* LARGE STACK MODEL <64K FOR STM8 COMPILER
* Copyright (c) 2006 by COSMIC Software
*/
#pragma space () @near
#pragma space * () @near
#pragma space const []
#define __MODSL0__ 1
#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\modsl0.h:1 FlexLM No such feature exists.
2019-05-21 1:58 PM
It seems to be a Cosmic license issue. Did you get the free license file from Cosmic company? When you install the free tool into a new workstation you have to communicate the PC data to the software house, they will answer with a new license file.