cancel
Showing results for 
Search instead for 
Did you mean: 

connection proxy error and no STM32 In DFU mode connected

amr5
Associate

hi guys i am trying to use  STM32MP135x-DK board with STM32CubeProgammer but after opening the software i got no internet connection  due to proxy setting and also no the program does not see any dfu device connected through usb .. can anyone help with this ? 

 

2 REPLIES 2
amr5
Associate

i forgot to mention that i am using ubuntu 22.04

PatrickF
ST Employee

Hi @amr5 

1) proxy message is likely because you have access to internet thru a proxy. Please check CubeProgrammer documentation to setup a proxy (there is a menu in 'Help -> Proxy settings)

2) no DFU is not normal.

- Did you connect the right USB to the board (it is not the STLINK one) ?

- Did the board in DFU mode (check BOOT pins)

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.