cancel
Showing results for 
Search instead for 
Did you mean: 

when launching stm32cubeprogrammer i get the error: Exec error: No such file or directory

vbuon.1
Associate III

hi,

if i start the programmer from its bin directory then it starts w/ no problems. however, if i start the programmer outside of its bin directory then i get the 'No such file or directory' error.

when the programmer launches successfully there is an extra line printed on the terminal:

jar:file:/opt/st/stm32cubeprogrammer_2.7.0/bin/STM32CubeProgrammerLauncher!/fxml/Config.fxml

when it does not start then this line is not printed and instead the error message is printed.

any suggestions would be appreciated.

thanks,

vince

4 REPLIES 4
Houda GHABRI
ST Employee

Hi vbuon.1,

can you please give the command line used to launch CubeProgrammer?

Houda

hi,

thank you for your reply.

i type in the following:

STM32CubeProgrammerLauncher

thanks,

vince

Houda GHABRI
ST Employee

Hi vbuon.1,

You need to execute the script STM32CubeProgrammer located in the same directory of the launcher .

Please try and tell me if it is OK.

Houda

vbuon.1
Associate III

hi,

thanks for your suggestion.

the script failed bc the last line didn't have $DIR in front of 'jre/bin/java'. or, it didn't have 'cd $DIR' before the last line.

after i prepended '$DIR' to the last line i was able to launch the programmer

btw, what is this line that gets printed to the terminal by the programmer:

.jar:file:/opt/st/stm32cubeprogrammer_2.7.0/bin/STM32CubeProgrammerLauncher!/fxml/Config.fxml

thanks,

vince