cancel
Showing results for 
Search instead for 
Did you mean: 

How do I install this on Mac Big Sur 11.4 ?

LHarm.1
Associate III

I download the package onto my Mac in the Download folder.

I open a terminal and navigate to the Download/en folder.

I execute the command "./SetupSTM32CubeProgrammer-2.7.0.app/Contents/MacOs/SetupSTM32CubeProgrammer-2_7_0_maco"

I receive a popup window saying “SetupSTM32CubeProgrammer-2.7.0.app�? cannot be opened because the developer cannot be verified." Move to trash or cancel.

What am I doing wrong?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Houda GHABRI
ST Employee

Hi LHarm.1 

There is some tips in CubeProgrammer user manual to installl it on MAC:

  • Make sure you have administrator rights, then double-click SetupSTM32CubeProgrammermacos application file to launch the installation wizard.
  • In case of error, try one of the following fixes:  $sudo xattr -cr ~/SetupSTM32CubeProgrammer-macos.app  launch the .exe file with the command sudo java -jar SetupSTM32CubeProgrammer-2.7.0.exe.

can you please try them and tell me if it is Ok?

Houda

LHarm.1
Associate III

The app installed, but does not run.