cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L562EDK board can't be connected to st linker,the keill also says cpu locked up stop target!

Ypeng.1
Associate

I am working on the stm32l562 DK Board, when I program Software into STM32L5 microcontroller internal Flash memory and Configure STM32L5 static security protections, I find that stm32l562 DK Board can not conect to the stlinker with stm32cube programmer.at the same time the keil says cpu locked up ,stop target.

if I want to connect to the stlinker,what I can do?

stm32l562 DK Board

stm32cube programmer and keil

thanks

1 REPLY 1
Houda GHABRI
ST Employee

Hi @Ypeng.1​ ,

Sorry for the delay.

Can you try to connect the board in hot plug mode and tell me if it's ok?

regards,

Houda