2020-09-26 12:43 AM
Hello STM team,
I am working with STM32L562E-DK.
It was working fine, but suddenly the STM32L562E-DK is failing to connect. And generates a FAIL.TXT which says "The interface firmware FAILED to reset/halt the target MCU".
NOTE: I have not done any modifications so that it gets affected.
Please give me suggestions for the same.
Thank you in advance!!
2020-09-27 02:57 PM
Hello @Neel
Tried to upgrade the firmware with STM32CubeProgrammer, set to "Connect Under Reset" mode and erase the whole MCU.
Check also the jumper settings.
Hope this helps you.
Imen