cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F412RE Flash 512KB OVER SIZE?

KMin .1
Associate II

HI.

The STM32F412RE flash memory size is 512 kB.

Why 1024 KB is accessible.

write and read successfully.?

0693W00000YAJaOQAX.png

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hello @KMin .1​ 

Even if you are able to use 1024KB of flash on STM32F412RE, only 512kB is tested by ST. So we cannot guarantee the behavior in the whole 1024KB of the flash.

When your question is answered, please close this topic by choosing Select as Best the answer that answered your question or solved your problem. This will help other users find that answer faster. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
KnarfB
Principal III

Probably the same die as similar MCUs with more flash, but not fully functional / tested under all conditions.

hth

KnarfB

FBL
ST Employee

Hello @KMin .1​ 

Even if you are able to use 1024KB of flash on STM32F412RE, only 512kB is tested by ST. So we cannot guarantee the behavior in the whole 1024KB of the flash.

When your question is answered, please close this topic by choosing Select as Best the answer that answered your question or solved your problem. This will help other users find that answer faster. 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.