Question
Problem with V2.17.0 and STM32G491, Erasing Too Many Sectors
- September 10, 2024
- 4 replies
- 1112 views
STM32CubeProgrammer version 2.17.0
Target STM32G491, device ID 0x0479, 512KB flash
When loading a large hex file (284kB), the programmer tries to erase 65293 sectors! There's only 256 sectors in target, and the image only needs 141 sectors erased.
We also use the internal flash to storage some settings of the device. These settings are erased when using version 2.17.
We tried this earlier with version 2.13 and no problem was detected.
See attached log files of both version 2.13 and 2.17
Please provide help.
Thanks,
EG