2018-04-11 1:08 AM
Fails to use stm32cubeprogrammer for stm32f765?
What can be wrong?
#stm32cubeprogrammer2018-04-12 11:51 PM
Hi!
I have attached a hexfile. It did not work with stmcubeprogrammer.
This is a the new file.
The old and the new file work with older st-link utility program.
They also work with the CAN bootloader.
Hex files were created with IAR.
/Conny
2018-04-17 5:47 AM
Not solved... Help!!!
2018-04-17 6:59 AM
Hi
Olander.Conny
, Hist.mcu
,To share also with STCommunity the exchanges I have within ST online support (as supporter).
Setup ofOlander.Conny
is using an STM32F765ZG, i.e. with the 1MB Flash configuration. This was not supported by default out of the box from the STM32FlashLoader V2.9.0RC8, but I was able to provide previously an associated .STmap configuration file to make it work.If I look at the STM32CubeProgrammer database (in C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\Data_Base file STM32_Prog_DB.xml), I am only seeing the 2MB single and dual banks flash configuration for the STM32F76x/STM32F77x (with Device ID 0x451).
This explains,
st.mcu
, why it is working for you on the STM32F769I-Discovery (since including aSTM32F769NIH6 microcontroller featuring 2 Mbytes of Flash)So for me, we have the same issue as for the STM32FlashLoader, we need to add inside STM32CubeProgrammer a 1MB Flash configuration to STM32F76x/STM32F77x Device ID 0x451 covering STM32F765xG products .
Best regards,
Cedric2018-05-17 11:32 PM
When are the utdate available?
2018-06-01 5:33 AM
Why can you not just fix this?
2018-08-27 6:49 AM
Hello,
Please note that the issue explained by Cedric was fixed in STM32CubeProg V1.1.0.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-01-13 11:20 PM
Hi!
This still does not work, When comes the stmcubeprogrammer update that fixes this problem?
/Conny
2020-09-14 4:27 AM
Hi!
It still does not work...
I Have tried cubeprogrammer v2.50 today and the errors remains...
When can this be fixed?
/Conny
2020-09-14 6:51 AM
Fixing issues and basic functionality with these applications seems to be a problem for ST.
I've reported several issues with HEX and ELF parsing issues, including ones which break the external loaders, which don't seem to get addresses or tested throughly. ie issues with one file might be changed, but systemic issues with other files is not.
Needs independent code review and oversight.