2018-04-11 1:08 AM
Fails to use stm32cubeprogrammer for stm32f765?
What can be wrong?
#stm32cubeprogrammer2018-04-11 2:21 AM
Hi
conny
,Why are you marking this question as 'Assumed answered'?
Did you already resolved the issue you have?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-04-11 5:37 AM
Hi!
It is not resolved.
How can I remove the marking 'Assumed answered'?
/Conny
2018-04-11 5:39 AM
It works in stlink, see attached file. Same hex file, same address...
2018-04-11 7:19 AM
I think that's Jive's heuristics at work, the OP didn't mark anything correct.
Looks like the Cube Programmer doesn't understand the 0x00200000 mapping of the FLASH. There is perhaps a linker script setting to map it better so as to avoid the error.
2018-04-11 7:36 AM
I don't think it is a Jive's issue; the OP may mark his question as assumed answered clicking on:
Unfortunately, there is no way even for moderators to unmark it. So we have to look for the answer now .
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-04-11 10:23 AM
In the full editor you should be able to post images with the camera icon rather than as attachments.
2018-04-12 12:42 AM
I have fixed the attachment now. Same hexfile worked with st-link program...
2018-04-12 4:43 AM
I have not solved this problem, any ideas?
2018-04-12 7:26 AM
Hello,
I have an STM32F769I-Discovery and I generated a .hex from one example available in the CubeF7 package (GPIO_EXTI), then I was able to load it successfully with STM32CubeProgrammer.
Could you please retry again from your side with another .hex?
If the issue is related to your initial .hex file, may it be possible for you to share it (even in PM) for farther check from our side?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.