cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer v2.19.0 USB DFU does not complete the connection

Hans T
Associate III

 

 

Hello,
There seems to be a bug in Stm32CubeProgrammer v2.19.0

I connect the STM32F767 with USB1 (DFU).

When I press the CONNECT button, the connection stops at  44 bytes.

the connection is "Not connected"

however, I can now download a program.

 

stm32.JPG

1 REPLY 1
STOne-32
ST Employee

Dear @Hans T ,

Can you type in Read Address the RAM address @0x20000000 :  and see/send  the message/log after reading ? 

Thank you.

 

STOne-32.