Skip to main content
Associate
Mar 17, 2025 7:20 PM UTC
Solved

Can't connect to STM32H755 after changing boot option byte

Hello,

after changing one of the BCM4/7 boot option bytes of my Nucleo STM32H755 board with STM32CubeProgrammer, I can't connect to the MCU any more. When trying to connect with STM32CubeProgrammer, I get

Error: Unable to read device id from ROM table

Error: ST-LINK error (DEV_CONNECT_ERR)

 

Is this related to the change in option bytes or did the board get damaged somehow?

Thanks and regards,

Martin

This topic has been closed for replies.
TDK
TDKBest answer
Mar 17, 2025 8:24 PM UTC

Try connecting using access port 3 instead of access port 0.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
TDKBest answer
Mar 17, 2025 8:24 PM UTC

Try connecting using access port 3 instead of access port 0.

"If you feel a post has answered your question, please click ""Accept as Solution""."
mt7883Author
Associate
Mar 18, 2025 7:25 AM UTC

Wow, this works, thanks a lot!

I just double checked: When I turn option BCM7 back on I can connect again on port 0. When I turn BCM7 off I can only connect on port 3.

mƎALLEm
ST Technical Moderator
Mar 18, 2025 8:39 AM UTC

Hello @mt7883 ,

Read this new article.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.