2022-07-20 4:17 AM
Dear all
I think the description is wrong or BOOT0/BOOT1 is swapped - see attachments.
If the option bytes are programmed as shown under STM32CubeProgrammer.png, the controller boots from flash.
Thanks in advance,
Franz
2022-07-20 7:04 AM
Yes they are. I found out the hard way when it did not work. It was pointed out to me to use the documentation (Reference Manual) and that works.