cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.9.0 released

Nawres GHARBI
ST Employee

New features

• Updated the programming mechanism for the STM32U575/585 microcontrollers via a flash loader usage in TZEN = 0, and a new programming mode in TZEN = 1 (fast/reliable)

• Added double authentication and user keys provisioning via JTAG for the STM32WB Series (feature only available with bootloader in previous versions)

• Added a scripting mode including the existing STM32CubeProgrammer CLI commands and a new macro for data manipulation

• Added the support for the PKCS#11 protocol in the signing tool (STM32MP1 Series).

• Added the support for Microsoft® Azure® RTOS USBX DFU stack

Fixed issues

110368 STM32L5 RSSe binary must be renamed as it handles both the JTAG and bootloader.

110531 [FUS] Upgrade problem with STM32CubeProgrammer of stm32wb5x_FUS_fw.bin version v1.2.0 on STM32WB55RE (512 Kbytes).

111044 Programming issue using STM32L486xx microcontrollers connected via USB.

111417 Changing secure area errors.

112266 Debug in Low-power mode does not display the right state of Stop bit.

112484 New ST-LINK firmware release V3J8M3 should limit bandwidth to 1 MHz on GUI.

112545 CLI does not read all requested upload sizes.

113605 [CLI] Erase all not possible using UART.

113806 [OB] Error message when configuring WRP option byte.

114171 STM32CubeProgrammer fails to program large segmented .hex file to external Flash memory.

114893 [STM32G4] Bit SEC_SIZE1[8] cannot be programmed.

115651 Issue with option bytes IWDG and WWDG for STM32G07xxx devices.

116070 Programmer failed to load bin on STM32U5 with newer ST-LINK firmware version.

Link

https://www.st.com/en/development-tools/stm32cubeprog.html#overview

3 REPLIES 3
BBeck.1
Associate II

I'm connected to a STM32MP1-discovery kit, my IDE prompted for STlink fw upgrade, now I cannot connect via DFU (usbc). Anyway to back out of fw update?

Marcuka
Associate III

Hi,

need urgent help using the C++ api. You can read my problem here:

https://community.st.com/s/question/0D53W00000znxDiSAI/cant-use-stm32cubeprogrammer-api

I'm using Win 7/64 and build the 64 bit version of the Visual studio project.

Furthermore I'm unable to open the help file or uninstall the product. What you can advice me?

Any help is highly appreciated!

Hi @Marcuka​,

It looks like your question is answered, right?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.