User Activity

Hi,I need more 4kB of flash memory. Can I achieve this easily and safely by removing some not used functionality in the I-CUBE-LRWAN project?I suppose Lorawan Class B and C featues will not be needed. Can I just exclude this files from the project an...
Posted on February 09, 2018 at 15:52   Hello! I want to program a STM32L073CB device FLASH and option bytes and then to start the application. If I don't program the option byte I have not problem with the application start. That is the command line...
Kudos given to