2020-08-31 04:51 PM
I have installed Java:
Successfully installed STM32CubeProgrammer:
If i launch in finder CubeProgrammer quits
If i launch in terminal java quits
I currently have STM32CubeIDE, STM32CubeMX, STM32CubeMonitor and STM32CubeMonitorRF all installed and working correctly.
Does anybody have any suggestions for a solution? I know this issue has been reported by a number of other community members using older software versions.
Solved! Go to Solution.
2020-10-08 02:33 PM
2020-09-02 06:57 AM
Hello @Community member
Thanks for the feedback, issue reported to the tool development team that will plan the correction.
Best regards,
Nesrine
2020-09-08 10:44 PM
Any update I'm having the same issue?
2020-09-12 11:31 PM
I believe I'm encountering the same problem on Ubuntu 20.04:
./STM32CubeProgrammer/bin/STM32CubeProgrammer
Error: Could not find or load main class com.st.app.Main
Caused by: java.lang.NoClassDefFoundError: javafx/application/Application
2020-09-13 02:07 PM
@Community member
I also had problems starting it, but with some help it finally worked (macOS only)
Please check that thread. https://community.st.com/s/feed/0D53W00000GWcmTSAT
Hope that helps.
2020-09-13 02:08 PM
@Nesrine.JLASSI
Hi there.
Is there any chance that this tool gets promoted to more modern JDK?
2020-10-01 11:28 AM
I'm having same issue - installed various versions of JDK - currently on 8.0_231 - and no matter which version of java I use or how I launch SetupSTM32CubeProgrammer-2_5_0_macos (either via .app or command line) I get the following:
Last login: Thu Oct 1 12:12:17 on ttys003
/Users/chucka/Downloads/en.stm32cubeprog_v2-5-0/SetupSTM32CubeProgrammer-2.5.0.app/Contents/MacOs/SetupSTM32CubeProgrammer-2_5_0_macos ; exit;
chucka@MacBook-Air-5 ~ % /Users/chucka/Downloads/en.stm32cubeprog_v2-5-0/SetupSTM32CubeProgrammer-2.5.0.app/Contents/MacOs/SetupSTM32CubeProgrammer-2_5_0_macos ; exit;
Error: Unable to access jarfile ../../../SetupSTM32CubeProgrammer-2.5.0.exe
[Process completed]
Any suggestions on how to get this thing installed?
2020-10-08 02:24 PM
I'm also having issue....
https://community.st.com/s/question/0D53W00000KHlCKSA1/installintg-cubeprogrammer-java-issue
2020-10-08 02:31 PM
Hello @LBeau.1
The root cause of this issue may be conflicts between Java versions, so please, if you have many java versions installed try to uninstall all except 1.8.0_26 and then re-install CubeProgrammer.
Best regards,
Nesrine
2020-10-08 02:33 PM
It worked, see the update.
https://community.st.com/s/question/0D53W00000KHlCKSA1/installintg-cubeprogrammer-java-issue