cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.4.0 released

Nawres GHARBI
ST Employee

New features

• Added the support of the graphic user interface (GUI) for the firmware upgrade service (FUS) and stack upgrade for the entire STM32WB Series

• Support of HSM V2 on all STM32 microcontrollers and microprocessors supporting SFI/SSP

Fixed issues

77015 STM32CubeProgrammer cannot connect ST-LINK without the mass storage feature. 78350 STM32CubeProgrammer issue with STM32G0 when programming binary (size 18448 bytes).

Known problems and limitations

• For the STM32L5 Series, the connection via the ST-LINK protocol is allowed only when mode is set to hotplug with TZEN=1.

• For the STM32L5 Series, the Option Byte programming GUI is not intuitive enough. Refer to the STM32L552xx and STM32L562xx advanced Arm®-based 32-bit MCUs reference manual (RM0438) for permitted accesses.

• For STM32L4Pxxx and STM32L4Qxxx devices, Option Byte programming via bootloader interfaces presents some limitations.

• For STM32H7Axxx and STM32H7Bxxx devices, Option Byte programming via bootloader interfaces (USB) presents some limitations.

• STM32L5 series programming presents limitation in macOS® when TZEN=1 and RDP=0x55.

• With some small-screen resolutions, the graphical interface of STM32CubeProgrammer presents anomalies such as inaccessible buttons.

• Display issues depending on the monitor used can occur with Linux®.

• SFIx on STM32H743/753 devices fails via the debug interface.

• SFI-HSM V2 get certificate fails with STM32L462xx devices.

• Parallel Flash programming fails in macOS® for microprocessors in the STM32MP1 Series

Link:

https://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-programmers/stm32cubeprog.html#overview

12 REPLIES 12
Joerg Wagner
Senior III

Hello.

I use STM32CubeProgrammer 2.4.0 on MacOS Mojave (10.14.6).

No ST-Link is detected. I tried 3 different NUCLEO-F767I (one new board).

A long time ago I had no problems with version 2.1.0.

I can do nothing, no board access and no firmware upgrade.

What is missing or wrong?

Joerg

Same problem with version 2.2.0 of STM32CubeProgrammer.

The problem was the USB cable. One data line has a defect probably.