2024-07-08 01:42 AM
STM32CubeProgrammer v2.17.0 release information
New features:
• Added the support for the STM32MP25xx microprocessors in the STM32MP2 series
– Flash memory and OTP programming, SSP support
STM32WB07 MCU, and STM32WB09 MCU product lines
– Flash memory and OTP programming via debug and UART
– Key generation, software signature, and OTP provisioning
memory
– Flash memory and OTP programming via debug and UART
Refer to the STM32CubeProgrammer software description user manual (UM2237) for details.
Fixed issues:
126305 [GUI][STM32U5] RDP regression with password level 2 not working on all operating systems.
129215 [STM32CubeProg] Add new features: save and load OB configurations.
136058 [STM32U575ZI] STM32CubeProgrammer bug affecting flash memory programming when flash memory
banks are swapped.
143616 [STM32CubeProg] Need to update the nswab_BANK description according to the new reference manual
changes.
152836 [Flash loader][STM32CubeProg][STM32H5] When SWAP_BANK is enabled, bank 1 erasing is not functional.
168475 [STM32G4][GUI/CLI] Wrong description of BOOT_LOCK option byte.
171718 [STM32WL5x] An external flash loader generated with STM32CubeIDE does not work with
STM32CubeProgrammer.
172137 Invalid .elf file if the path uses valid UTF-8.
172961 [DATABASE][D415] Programming failure via the bootloader interface in the second bank of a 1‑Mbyte target.
175709 [UART] Sending an additional page to be erased.
175852 [Bootloader] Programming at the address 0x0Cxxxxxx via the bootloader interface.
175981 [DATABASE][D492] Wrong multiplier for SECW option bytes via the bootloader interface.
178135 STM32CubeProgrammer fails to program via the USB.
179072 [STM32C0][0x443] Missing configuration in database for device ID 0x443 with 16 Kbytes of flash memory.
179216 [API] Deallocate memory after read.
180037 Calling the obDisplay API crashes
Known problems and limitations:
– STM32H7 microcontrollers: support integrity check for SFI/SMI:
◦ Only the devices with a bootloader version higher than 0x91 are supported.
◦ STM32CubeProgrammer does not support the devices with older bootloader versions. Users
must use STM32CubeProgrammer v2.9.0 to use devices with old bootloader versions.
– STM32H73xxx microcontrollers: support integrity check for SFI/SMI/SFIx:
◦ Only the devices with a bootloader version higher than 0x93 are supported.
◦ STM32CubeProgrammer does not support the devices with older bootloader versions. Users
must use STM32CubeProgrammer v2.9.0 to use devices with old bootloader versions.
– STM32H7Bxxx microcontrollers: support integrity check for SFI/SMI/SFIx:
◦ Only the devices with a bootloader version equal to or higher than 0x92 are supported.
◦ STM32CubeProgrammer does not support the devices with older bootloader versions. Users
must use STM32CubeProgrammer v2.9.0 to use devices with old bootloader versions.
– The SPI interface quits after starting without a connection.
– Option byte issue: impossible to decrease the RDP from the BB to AA state.
– The .hex file does not modify the WRP and PCROP option bytes of bank 2 for the devices with
512 Kbytes of dual-bank flash memory.
– Unable to change the option bytes when WWDG_SW and IWDG_SW are unchecked.
– STM32CubeProgrammer fails to download via J-Link
– STM32G491xx microcontrollers: Issues occur when erasing sectors in bank 2 memory
– Unable to read, write, or erase the external flash memory when TZEN is enabled
– STM32CubeProgrammer does not support combined SFI and SMI.
– SMI programming fails.
– SFI is not supported.
– Erasing the external flash memory is not supported using IWDG.
– GUI: the external memory edition is not supported via USB and UART while connected to the
OpenBootloader.
– Option bytes are not supported via OpenBootloader interfaces.
– SSP secret generation is not supported
– Impossible to modify the unlock_2b option byte value when programming the OB list.
– STM32U535/545 microcontrollers: SFIx is not supported.
– STM32U575VGT6: the start address of Flash-Bank2 is incorrect.
– STM32U59xxx microcontrollers: SFIx only supports the area E installation with OTFDEC region 1
(region 0 on TPC).
– STM32U59xxJ, STM32U5AxxJ, STM32U5Fxxx, and STM32U5Gxxx microcontrollers: wrong sector
size when DBANK is equal to zero
– STM32U5Fxxx and STM32U5Gxxx microcontrollers: SFIA not supported via SPI.
STM32WBA microcontrollers:
– OpenBootloader via SPI: cannot connect to STM32CubeProgrammer when the baud rate is below
3000 Bd.
– “Connect Under Reset” is not working when called by STM32CubeIDE.
Refer to the STM32CubeProgrammer Release note (RN0109) for further details.
Download Link: