cancel
Showing results for 
Search instead for 
Did you mean: 

STM32Cube Programmer API USB Example error

Gabriel T
Senior

Hello,

I put my STM32H743XI in Bootloader mode and launch STM32Cube Programmer USB example on VS and got :

0693W0000059bznQAA.pngI have two question :

  • Where does this error comes from and how to fix it ?
  • Can I skip option bytes programming and still flash my MCU ?

Regards

1 ACCEPTED SOLUTION

Accepted Solutions
Mike_ST
ST Employee

Are you talking about the warning on BOR level not being updated ?

If so, it is not an error and you can skip it if you don't need to program the BOR Level.

View solution in original post

1 REPLY 1
Mike_ST
ST Employee

Are you talking about the warning on BOR level not being updated ?

If so, it is not an error and you can skip it if you don't need to program the BOR Level.