2023-07-12 2:23 AM
Hi,
I'm having an STM32L4P5.
In sectors [0 7] there is a bootloader, in sectors [8 75] the application is located.
With STM32_Programmer_CLI.exe I can issue an erase for specific sectors and it seems to work. But STM32_Programmer_CLI.exe wants to programm all the time beginning with sector 0. That doesn't matter for the bootloader, but programming the application overwrites the bootloader. --skiperase is not an option, because STM32_Programmer_CLI.exe still tries to programm the application at sector 0, and since it isn't erase, it fails.
I would need an option for excluding sectors from programming.
Tx
Matthias
2023-07-12 2:29 AM
Do you have the latest programmer version? Similar bugs have been reported here, may be fixed in the latest update.