cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with J-LINK Plus to flash a .bin file again to STM32WBA55CG

ledi7
Associate III

Hi,

after flashing the binary files of BLE_ApplicationInstallManager and BLE_p2pServer_ota on the STM32WBA55CG, I can no longer access the controller.

What i did:

  1. Flashing .bin file of the BLE_ApplicationInstallManager @ start address 0x0800 0000
  2. Flashing .bin file of the BLE_p2pServer_ota @ start address 0x0800 6000

Result: Flashing ok and programm is working

Then I changed the settings in STM32_WPAN configuration (Change BLE Stack from Basic to Full). I generated the code and compiled it.Then I tried to flash the new .bin file of the BLE_p2pServer_ota @ start address 0x0800 6000 and got this message:

2025-01-26_09h33_28.png

However, the controller (STM32WBA55CG) is not listed in the settings:

2025-01-26_09h33_58.png

And therefore, I am no longer able to establish a connection to the controller with STM32CubeProgrammer:

2025-01-26_10h08_48.png

I also checked the COM port, but everything (J-Link on COM7) looks fine here:

2025-01-26_10h10_04.png

Then I tried to establish a connection with STM32CubeIDE, but that also failed:

2025-01-26_10h06_56.png

 

Does anyone have any ideas what I can do?

0 REPLIES 0