cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with STM32G0B0: failed to download Segment[0]

I have a Nucleo board with a new MCU, base board is the Nucleo-G070RB. Now it is a ST link with a STM32G0BORE.

I have a problem with the internal bootloader where i cannot upload a new program via USB DFU.

There is no hardware problem because VCP works just fine. No data corruption of something.

I have tried .HEX .BIN and .ELF all have the same problem.

This is the error log is have:

18:04:57 : UR connection mode is defined with the HWrst reset mode

 18:04:57 : USB speed  : Full Speed (12MBit/s)

 18:04:57 : Manuf. ID  : STMicroelectronics

 18:04:57 : Product ID : DFU in FS Mode

 18:04:57 : SN     : 204E315A4630

 18:04:57 : DFU protocol: 1.1

 18:04:57 : Board    : --

 18:04:57 : Device ID  : 0x0467

 18:04:57 : UPLOADING OPTION BYTES DATA ...

 18:04:57 :  Bank     : 0x00

 18:04:57 :  Address    : 0x1fff7800

 18:04:57 :  Size     : 68 Bytes

 18:04:57 :  Bank     : 0x01

 18:04:57 :  Address    : 0x1fff7870

 18:04:57 :  Size     : 4 Bytes

 18:04:57 : UPLOADING ...

 18:04:57 :  Size     : 1024 Bytes

 18:04:57 :  Address    : 0x8000000

 18:04:57 : Read progress:

 18:04:57 : Data read successfully

 18:04:57 : Time elapsed during the read operation is: 00:00:00.031

 18:05:05 : Memory Programming ...

 18:05:05 : Opening and parsing file: g0b0test.hex

 18:05:05 :  File     : g0b0test.hex

 18:05:05 :  Size     : 42.56 KB 

 18:05:05 :  Address    : 0x08000000 

 18:05:05 : Erasing memory corresponding to segment 0:

 18:05:05 : Not flash Memory : No erase done

 18:05:05 : File segment @0x08000000 is not 255-bytes aligned. It will be aligned to @0x07FFFFF8

 18:05:05 : Download in Progress:

 18:05:05 : Error: failed to download Segment[0]

 18:05:05 : Error: failed to download the File

 18:05:05 : RUNNING Program ... 

 18:05:05 :  Address:   : 0x08000000

 18:05:05 : Start operation achieved successfully

 18:05:06 : Warning: Connection to device 0x467 is lost

 18:05:06 : Disconnected from device.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi @PieterInHetBos,

Can you please check Option Byte setting?

Try this workaround: Force to erase 'entire flash' memory, before start debugging.

Can you please share the Option Bytes parameters and the log file, in order to investigate the issue.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

15 REPLIES 15
Imen.D
ST Employee

Hello @PieterInHetBos​ and welcome to the Community :)

Could you please try to use STM32CubeProgrammer on standalone.

Make sure to use latest release of CubeProgrammer, and try to upgrade ST-LINK firmware.

Check the registers and ensure that “flash empty�? is not causing such issue.

I advise you to erase the flash memory first.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

A code, which expects a 255-byte alignment, is definitely broken:

https://community.st.com/s/question/0D53W00002CMICqSAP/stm32cubeprogrammer-213-bugs

Hello Imen,

Thank you for your reply.

I have updated CubeProgrammer to V2.13 and CubeIde V1.12. I have updated the STLink firmware. I also have erased the memory everything is filled with FFFFFF.

What needs to be the Option Bits on the STM32G0B0RET?

Kraal
Lead

Hi Imen,

It seems that the 0x467 loader is really broken. The bigger problem is that CubeIDE is also relying on it to load the program before debugging, and it is now impossible on some of the G0 devices.

This must be fixed as soon as possible...

Best regards,

Kraal

Hello Imen,

I have downgraded to STMCubeIDE to 1.7 with STMCubeMX 6.3 and STMCubeProgrammer 2.8. This fixed all the problems. Please fix the new software so we can use the updates

Imen.D
ST Employee

Hi @Kraal​, Hi @PieterInHetBos​ ,

Our team is very aware of this issue now and working to fix this in the coming release.

An internal ticket ID 149042 is submitted in order to improve the tool.

(PS: ID 149042 This is an internal tracking number and is not accessible or usable by customers).

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Dear Imen,

Any luck on a update?

Hi @PieterInHetBos​ ,

The fix is integrated and will be published in the STM32Cubeprogrammer v2.14.0.

But, for the moment I can't give you any information about delivery date.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Thank you, i will use the older version for now. I works for now, thank you very much!