2024-03-27 8:04 AM
Hi,
I have 20 boards in a 4x5 panel board. all boards have the same MCU. is it possible to program all boards via a panel at the same time? if so, how can I do that? which software and hardware tools do I need?
Thank you.
2024-03-27 8:38 AM
Read AN2606
2024-03-27 8:42 AM
SWD doesn't daisy chain
JTAG could potentially, but you'd need the right equipment and software. Decide how many connectors/pods you want to attach to the panel, how many devices you want to chain. Failure of one might preclude cascading to others.
If you route power, and BOOT0 / RESET over the panel, and expose a UART you might be able to implement AN3155 UART protocol
You could perhaps chain devices that allow one to program the next.
Really going to be a function of you creativity, understanding the protocols, and options.
See also AN2606