cancel
Showing results for 
Search instead for 
Did you mean: 

Mac OS X Cannot Connect to Target - Target Voltage Shows .98

PMona
Associate II

I have succesfully installed STM32Cube Programmer v1.0 and v1.21 for OS X on three Macs. One Mac is a 2011. The other two are much newer. On the newer Macs the software detects the ST-LINK but shows the target voltage as .98V. On the old 2011 Mac, the target voltage is shown as 3.3V.

I can connect to our PCB and load the Binary via SWD using the 2011 Mac, but I cannot connect to the target when using the newer Macs. After updating from V1.0 to V1.21, The issue is not related to the SW Version.

I have tried direct USB ports, powered hubs, etc. Multiple STLINKs, same USB cable.

I suspect this has to do with the lower target voltage, but I don't know why it would be lower.....Also don't know how to correct it.

Anyone else have this issue ?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0