cancel
Showing results for 
Search instead for 
Did you mean: 

Hi, I try to install STM32CubeProgrammer_2.10.0 on linux RH. Installation is OK but when I run I have error messages : on RH 7.8 is with GLX 1.2 version (because we must have 1.3 or >) on RH 7.9 (with GLX 1.4) Exception in Application start method

PLECU.1
Associate II

In RH 7.9 , Exception in Application start method (java.lang.reflect.InvocationTargetException)

3 REPLIES 3
Sara BEN HADJ YAHYA
ST Employee

Hello @PLECU.1​ ,

Could you please provide us with more information about the PC environment (processor, architecture... ) ?

Thanks,

Sara.

PLECU.1
Associate II

Hi Sara ,

It's a virtual Linux Red Hat machine in RH 7.8 .

Processeur Intel Neon 2,2 Ghz architecture x86_64

RAM : 32Gbs

Tanks for your help

PLECU.1
Associate II

Hi ,

I have testing installation on a new directory (with "root" account)

Installing is well , running STM32CubeProgrammer open the IHM (without possibility to resize the window) but when I want to run it from my $HOME (with my account user) , it doesn't open .

How can I run the installer (root or user ?) and run IHM STM32CubeProgrammer correctly (for all users) ?

thanks