2019-08-15 10:26 AM
Good afternoon, I was trying to debug a program on my new stm32f103C8T6 chip using the st-link v2 programmer, but i always get the same error : Error: failed to erase memory
I have tried the procedure with multiple boards so i guess that the problem is software, here is the full console output :
STMicroelectronics ST-LINK GDB server. Version 5.2.3
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_k3pQvR.log
ST-LINK SN : 33FF6D064E59343942520343
ST-LINK FW : V2J33S7
Voltage : 3.20V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x410
Device name : STM32F101/F102/F103 Medium-density
Flash size : 63.999 MBytes
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_JSWBJu.srec
File : ST-LINK_GDB_server_JSWBJu.srec
Size : 9716 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 9]
Error: failed to erase memory
Error: failed to erase memory
Encountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.0.0.201904021149/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Error! Failed to read target status
Debugger connection lost.
Shutting down...
Thanks !
2019-08-16 6:47 AM
You are probably right about not flakey connection since the funny looking value is always the same. Do you get the same value from all of your boards?
Look in the reference manual for your CPU. Find the "flash size register" and see its address. For example, for the STM32L4xx, it is at 0x1fff 75e0. I would expect it is in a different location for your F103. Run your programmer software of choice and have it read memory from that address. See what it shows. Again, for my L433 it shows 0xffff 0100. The 16 MSBs are ignored because the size register is only 16 bits wide. 0x0100 = 256K Bytes of FLASH.
2019-08-16 3:31 PM
@Bob S finally found the problem :
I went on Windows and attached the st link v2, started the program st-link and disabled 'read out protection' from configuration bits, once i did that, I could write freely any program on the flash using st-link command on mac OS and booting on System Memory (Boot<1:0> = 01).
Thanks all for your help !!
2019-08-19 8:47 AM
Don't forget to mark this as "answered' :)
2019-08-23 2:07 AM
I got the same error with STM32L151
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.1.0
-------------------------------------------------------------------
Log output file: C:\Users\Tonda\AppData\Local\Temp\STM32CubeProgrammer_a15552.log
ST-LINK SN : 0677FF564948897767025744
ST-LINK FW : V2J33M25
Voltage : 3.24V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x429
Device name : STM32L100x6xxA/STM32L100x8xxA/STM32L100xBxxA/STM32L15xx6xxA/STM32L15xx8xxA/STM32L15xxBxxA
Flash size : 27.125 MBytes
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a15552.srec
File : ST-LINK_GDB_server_a15552.srec
Size : 88948 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Error: Flash loader cannot be loaded
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.0.1\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.0.0.201904021149\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Error! Failed to read target status
Debugger connection lost.
==============================
Another interesting thing...
1) I cannot erase the chip with STM32CubeProgrammer
11:02:40 : STM32CubeProgrammer API v2.1.0
11:02:42 : ST-LINK SN : 0677FF564948897767025744
11:02:42 : ST-LINK FW : V2J33M25
11:02:42 : Voltage : 3.24V
11:02:42 : SWD freq : 4000 KHz
11:02:42 : Connect mode: Under Reset
11:02:42 : Reset mode : Software reset
11:02:42 : Device ID : 0x429
11:02:42 : UPLOADING OPTION BYTES DATA ...
11:02:42 : Bank : 0x00
11:02:42 : Address : 0x40023c1c
11:02:42 : Size : 136 Bytes
11:02:42 : Bank : 0x01
11:02:42 : Address : 0x1ff80000
11:02:42 : Size : 136 Bytes
11:02:42 : UPLOADING ...
11:02:42 : Size : 1024 Bytes
11:02:42 : Address : 0x8000000
11:02:42 : Read progress:
11:02:42 : Data read successfully
11:02:42 : Time elapsed during the read operation is: 00:00:00.007
11:02:49 : MASS ERASE ...
11:02:49 : Error: Mass erase operation failed.Please verify flash protection
2) but, I can erase it by STM32ST-LinkUtility
???
2019-08-23 2:10 AM
"Error! Failed to read target status"
I think that you must disable 'read out protection' in st-link utility, had the exact same problem
2019-08-23 2:29 AM
ooooooh, thanks, can you little bit direct me where to set it.
Thx Ant
2019-08-23 4:01 AM
try 'configuration bits', it's there, after having disabled it erase the flash memory and retry debugging using stm32cube if you want
2020-02-05 11:38 AM
I had something that looked quite similar using CubeMX IDE and a "Blue Pill":
I dowloaded Stm32Cube Programmer and discovered that RDP - Read Out Protection was set. So Flash Memory was read-protected. Unchecking this protection solved my issue (both with Stm32Cube Programmer and CubeMX IDE).
Go !
JMF
2020-09-28 9:24 AM
We are facing a similar problem on a L1-controller:
I have no idea, what the source of this error might be. Since flashing and executing the program are both working fine after using the older ST-LINK Utility, the issue should be located inside the Toolchain / STM32CubeProgrammer. The Read Out Protection is disabled (checked with ST-LINK Utility and STM32CubeProgrammer / CubeIDE can both read the flash and option bytes).
Please respond to this entry if you are facing the same problem or have any ideas to solve the issue.
2020-10-02 8:24 AM
If anybody else is experiencing the same issue as mentioned in my previous post:
For me it works not to use the STM32 Cube Programmer (GUI / CLI or integrated in Cube IDE).
I have switched to openocd (Windows x64 binaries), either by opening a Debugging server manually or integrating the server start in Cube IDE. This works perfectly fine. My platform:
Windows 10 64 bit
Cube MX / IDE / Programmer
STLINKV2/1
The problem occured with STM32L151CB-A and STM32L152CB-A.