2023-07-24 2:10 AM
opens this window:
whereas according to ST's website, current version is newer, 2.14.0:
Can you please comment on this.
Thanks,
JW
Solved! Go to Solution.
2023-08-01 1:53 AM
Hello @waclawek.jan ,
I have submitted a change request for the Updater redesign and will keep you updated on any progress or developments.
Internal ticket number: 158493 (This is an internal tracking number and is not accessible or usable by customers).
Sara.
2023-08-01 6:07 AM
Thanks @Sara BEN HADJ YAHYA .
JW
2023-10-06 3:23 AM - edited 2023-10-06 3:25 AM
I don't have a proxy server. I selected "no proxy" and I clicked "Test connection". Nothing happens. Updates don't work, I get "no connection" error.
2023-10-06 12:51 PM
I can get this one, but it freezes and doesn't work anyway.
And now at startup the application shows this:
But they cannot implement proper functionality even for such a simple message box! The OK and Cancel buttons both are just closing the message box. Why are there two buttons, if both do the same thing? And the window close button doesn't do anything at all - it doesn't even close the message box. So why is it active then? Or why doesn't it function as in normal software - doing the same as OK or Cancel, depending on the buttons present?
2023-10-27 1:51 PM
simply doesn't work. Do you suppose that I install a proxy server?
2024-07-24 6:28 PM - edited 2024-07-24 6:33 PM
Now I can't download it. After reading the license agreement and confirming, nothing happens. I tried using other browsers and also tried downloading different versions, but the result is the same.
Also, when trying to update from the program, I still can't do it.