2024-06-22 02:18 AM - edited 2024-06-22 05:59 AM
Hello,
i just installed the most recent version of Cube Programmer but when i click the Open File tab and select a folder the program crashes immediately. I'm running it in Windows 11 64-bit on an Acer laptop, i selected the correct 64-bit version for download.
It also crashes if i close the "Open file" dialog or click the Cancel button.
2024-06-22 02:26 AM - edited 2024-06-22 02:27 AM
Hi,
so maybe it cannot open any file ; in Win often a problem with "rights" (or antivirus, firewall)...
I would un-install, install in directory as it wants (and "allow" everything, if any question...).
And check in antivirus and firewall : app has all rights.
2024-06-22 02:53 AM
Thank you but i tried to turn off every protection and reinstall in the default directory c:\programs\, still crashing
2024-06-22 04:00 AM
So i have no "good idea" - (I use V2.15),
i would try: install old version, maybe V2.9.0 ... (there are some to try...) 🙂
2024-06-22 05:59 AM
I didn't notice there were old versions too, just tried to install 2.9 but no luck, still crashing :(